Unsupported Firmware

When WorkBench connects to a drive, it checks to make sure that the drive is executing a supported version of the drive firmware. If the firmware version is newer than WorkBench can recognize, the following warning is displayed.

Some features available in your firmware may not be fully supported by your WorkBench version. Choose one of the three options available on the warning screen:

Option Description
1 Provides link to download the latest version of WorkBench from kollmorgen.com.
2 Connects to the drive regardless of unsupported firmware.
3 Disconnects from the drive.

See Also

Invalid Firmware | Incompatible Firmware